Solar
Linking solar energy to the world's power needs, one cable at a time
Prysmian Group’s solar PV cable portfolio is composed of three brands:
- Prysmian PRYSOLAR – the newest global brand, designed to face the most unpredictable challenges and anticipate the future. It is compliant with international standards EN 50618/IEC 62930. Upgraded with enhanced water endurance.
- TECSUN - the premium brand made in Germany with over 15 years of experience and more than 1,000,000 km sold. This cable outperforms the standards of PV cables, is suited for the roughest conditions and for direct burial.
- SUNGEN – the regional brand for markets like North American with local standards such as UL/CSA The Group’s solar PV cables are designed for the interconnection of various elements in photovoltaic systems, including panel interconnection, between panels and combiner boxes or from combiner boxes to the inverter.