P-Laser

OVERVIEW

P-Laser

Prysmian offers the first fully recyclable and low-impact MV-cable insulation in the world.

P-Laser is a fully eco-friendly cable, manufactured using thermoplastic materials. It’s a recyclable solution that contributes to our customers’ sustainability work and drives added value for their business. 

The production process of this Medium Voltage Cable utilises ‘zero-gas’ technology, reducing CO2 emissions by around 1 tonne/km. 

Degassing is no longer required and its use of thermoplastics means a more efficient, fully integrated production process from start to finish.

HPTE

P-laser cables use HPTE (High Performance Thermoplastic Elastomer) insulation. It is PP based, characterized by a high flexibility, good thermo-mechanical properties, and excellent electrical behavior. 

The P-Laser insulation has a higher resistance towards developing water trees, cavities, and crystallization compared to XLPE . And even at very low temperatures, down to -25ºC, the HPTE material does have  a breakage extension of 300%.

HPTE thermoplastics also offers several other advantages:

  • Firstly: production is cleaner as a chemical process, the so-called crosslinking, is omitted. 
  • Secondly: P-Laser cables per mm of insulation are electrically stronger. 
  • Lastly: HPTE insulation is 100% recyclable after use.
OUR METRICS

P-Laser sustainability criteria

A major benefit of P-Laser insulation is that it doesn't require any crosslinking. This reduces the energy consumption of the P-laser manufacturing process, and eliminates the emissions of greenhouse gas-emissions associated with the XLPE cross linking process.Therefore, a cable with P-Laser insulation has a reduced CO2eq product footprint. Improved product circularity being thermoplastic instead of being crosslinked, the P-laser insulation is 100% recyclable at end of life. This is improving the circularity of this cable.

History of P-Laser

P-Laser is an innovation constantly developing and reaching new heights. We’ve constantly led the world in cable solutions and P-Laser is a further continuation of this commitment to innovation, representing a breakthrough in sustainability and performance.

An innovative cable insulation. P-Laser is a recyclable solution that contributes to our customers’ sustainability work and drives added value for their business. 

Choose P-LASER

Download our brochure now to explore how P-LASER can meet your needs and help you make a positive impact on the planet.

Made in Holland, delivered worldwide

Today, P-Laser is produced in the Netherlands for 10-52 kV, while 110 kV, 150 kV, 320 kV, 525 kV and 600 kV are produced in France and Italy.

In 2020, Prysmian had delivered almost 50,000 kilometers of MV P-Laser worldwide, with a total climate saving of more than 1,100 tons of CO2 Discharge. Additionally, 500kg of high-quality plastics can be recovered from every kilometre of P-Laser cable.

About E Path

We provide products that are the green life blood that brings energy and communications to homes, infrastructures and cities around the world.

With a business strategy consistent with the UN Sustainable Development Goals, we strive to be green inside. We express this through products that when installed in homes, infrastructures and cities around the world, make these just as green inside.

E Path goes beyond cables, embracing services and projects consistent with our strategy to be a solution provider.