Electric Vehicle Charging Infrastructure

Introduction

Toine Verschuur, Sales Director for Prysmian’s Draka products, presents the EVCS Hybrid Cable at Koninklijke Oosterberg’s “Dé Innovatie Kantine.” In this video, he explains how this innovative cable solution makes the installation of charging infrastructure easier, faster, and more efficient.

Draka EVCS Hybrid Cable Wins the Innovation price 2025

The Draka EVCS Hybrid Cable has won the Technische Unie Innovation Price 2025.

This smart, time‑saving solution makes EV charging installations easier and more efficient than ever, combining data and current.

Downloads

Manual EVCS Cable

08-2025

Prycharge EVC

04-2024

Protolon SC

11-2024

PRYCHARGE EVC

HULTA B3CA

11-2024

Selectiekaart EVCS

11-2024

Portfolio


Vulto Hulto B2ca

Vulto - Vulta

Installation cable for charging infrastructure
Download
Draka HULT EVCS Hybrid cable Desktop

HULT EVCS

Hyrbrid cable for EV charging stations
Tecsun Cable

Tecsun

High quality PV cable with TUV certification for connecting solar panels to converters
DOWNLOAD
draka-hult-evcs-hybrid-kabel

EVCS Hybrid

Hybrid cable for EV charging stations
DOWNLOAD

Emerging numbers of EV Chargers in the Netherlands

icon_reuse_sustainability

54,000+

Number of EV Chargers, 2024

icon circular materials

120,000+

Estimated Number of EV Chargers, 2028

icon_chemicals

122%

Incremental Growth in Number of EV Chargers, 2024 v.s. 2028

The energy transition and the future of renewable energy

icon_reuse_sustainability

537M

EV Charging Market Value, 2024

icon circular materials

1380M

Expected EV Charging Market Value, 2028

icon_chemicals

156%

Incremental Growth in EV Charging Market Value, 2024 v.s. 2028

FAQ

Find below our FAQ - common questions that tend to recur, for example, in seminars or through e-mails. If you do not find the answer to your questions, please contact us 

EV charging infrastructure (EVCI) refers to the network of electric vehicle (EV) chargers available for use. This includes public and private charging stations where EVs can be recharged, whether you are at home, work, or public locations such as shopping centers and highways. EV charging infrastructure is essential for supporting the growing number of EVs on the road, ensuring that drivers have convenient and reliable access to charging facilities.

The Netherlands has ambitious plans to expand its EV charging infrastructure. The Dutch National Charging Infrastructure Agenda aims to install 40,000 public charging points by 2025 and reach 1.7 million by 2030. Additionally, from 2025, around 550 new charging posts will be installed daily to create a nationwide network. These plans are part of a broader strategy to support the growing number of electric vehicles and ensure that charging infrastructure keeps pace with demand.

The EVCS cable simplifies the installation process by integrating the unique combination of power supply and communication functions into one cable. This innovative design reduces the number of cable entries into the charging stations, streamlining the installation and making it faster and more efficient. In addition, this cable ensures that less moisture or other substances enter the charging station. This minimizes potential problems in the long term and simplifies the connection of the charging station. This reduces the chance of errors and saves installation time.

The Hybrid EVCS cable from Draka consists of installation wires and 4-wire data cables for power supply and communication function in one.
Connecting the 4-core data cable works as follows;


The 4 cores have the color coding as a standard CAT cable, but 4 cores instead of 8 cores. The 4 cores have the colors orange/white, orange, green/white and green.
The order of connection is important for the performance of the cable. Connecting the cores should always be as follows;
Pin 1: Orange/white
Pin 2: Orange
Pin 3: Green/white
Pin 6: Green

To terminate the EVCS cable, use a CAT6a or CAT7 connector.

Pioneering The Electric Vehicle Revolution: The Growth of EV Charging Infrastructure (EVCI)

 

Imagine a bustling cityscape in the Netherlands, where electric vehicles (EVs) glide silently through the streets, seamlessly integrating into daily life. This vision is rapidly becoming a reality as the Netherlands is currently embracing a transformative journey towards sustainable transportation.

 

According to GlobalData, in 2024, the Netherlands proudly stands as a beacon of innovation with over 54,000 new EV charging stations dotting its landscape. These stations mean much more than just one of the components in the EV charging infrastructure (EVCI); they symbolize a commitment to a greener future. As the hum of traditional engines fades, the soft whir of electric cars takes over, powered by an ever-expanding network of EV charging points.

 

 

 

But this is just the beginning. By 2028, the number of EV chargers is expected to grow significantly, reaching an impressive 120,000 charging stations. In the meantime, the financial landscape of EV market also mirrors this physical expansion. The market value of the EV charging sector in the Netherlands is projected to soar from $537 million in 2024 to $1,380 million by 2028. This surge reflects the nation’s unwavering dedication to fostering an environment where electric mobility can thrive.

 

As the Netherlands leads the charge in Europe, it sets a powerful example of how a country can adapt and innovate to meet the demands of a sustainable future. The development of EV charging infrastructure in the Netherlands is a story of vision, growth, and an unwavering commitment to a cleaner, greener tomorrow.

 

Source: GlobalData

 

 

The right cable for every application

EVC (Electrical Vehicle Charging) cables: These are the flexible, durable cables that connect the charging station to the electric vehicle. Designed to withstand frequent use and various weather conditions, these cables are specifically engineered to safely transfer power from the station to the vehicle. It's important to note that this cable is vehicle-bound, meaning it's typically compatible with a specific type or range of electric vehicles.

 

EVCS (Electrical Vehicle Charging Station) cables: These are the crucial infrastructure cables that run from distribution stations to the charging stations themselves. They serve a dual purpose, providing both power and facilitating communication to the charging stations. What makes EVCS cables particularly noteworthy is our innovative design - we combine power supply and communication functions into a single cable. This unique feature offers several advantages: it streamlines the installation process, making it significantly faster and more efficient. Additionally, it reduces the complexity of the charging station setup, potentially lowering costs and minimizing the chances of installation errors. This integrated approach to power and data transmission represents a significant advancement in EV charging infrastructure technology.

PRYCHARGE

A super-fast charging infrastructure

Consumers want to feel reassured that charging stations are as easy to find and use as gas pumps. Hence, Prysmian is supporting the European Combined Charging System (CCS) as the global standard for charging electric vehicles. By offering the best EV charging cables on the market, we are able to back up the ultra-fast CCS-standard charging infrastructure enabling EVs to replenish for up to 400 km of range in only 15 minutes with powers ranging from 150 kW to 350 kW.

Trends

Electric transport is sustainable and rapidly developing. The Netherlands and Northern Europe are leaders in the field of electric transport. In order to be able to charge easily, a good charging infrastructure is needed. A good charging infrastructure means installing charging stations along motorways, in (residential) areas, at companies, hotels and shopping centres. The growing demand for charging stations means that the charging infrastructure needs to be designed in a smart and efficient way. Draka has innovative solutions, specifically for the rapidly growing electrical vehicle charging (EVC) market.

Contact Draka Team

Have a question for Draka? Here you will find all contact details of the Draka team. We are ready to answer your question.