MV E-LINE

OVERVIEW

Medium Voltage Cables with a Sustainable Core

MV E-LINE is Prysmian’s innovative portfolio of medium voltage cables designed with sustainability at heart. By integrating recycled materials and eco-efficient design, E-LINE helps reduce environmental impact while delivering reliable performance for energy networks, infrastructures, and industrial applications.

E-LINE innovations

Conductor

  • 10% recycled aluminum
  • Low carbon aluminum

Insulation

  • 100% recyclable P-Laser

Copper wire Screen

  • 100% recycled copper

Outer sheath

  • up to 98% recycled PE

P-Laser insulation

Prysmian offers the first fully recyclable and low-impact MV-cable insulation in the world

P-Laser is a fully eco-friendly insulation, manufactured using thermoplastic materials. It’s a recyclable solution that contributes to our customers’ sustainability work and drives added value for their business. 

The production process of this Medium Voltage Cable utilises ‘zero-gas’ technology, reducing CO2 emissions by around 1 tonne/km. 

Degassing is no longer required and its use of thermoplastics means a more efficient, fully integrated production process from start to finish.

SUSTAINABLE LOGISTICS

Minimizing footprint at every step

In 2022, Prysmian and Stedin launched a successful pilot project using electric heavy-duty vehicles for cable delivery—a first in the medium- and high-voltage sector. 

This zero-emission logistics approach is now the standard for all MV E-LINE deliveries, which contributes to reducing the carbon footprint throughout the entire lifecycle of the cable

SUSTAINABLE LOGISTICS

Cable Drum Management

ALESEA is an innovative IoT-based solution that transforms traditional cable reels into connected, trackable assets. By integrating RFID and GPS technologies, ALESEA provides real-time insights into reel location, usage, and condition—streamlining logistics and reducing inefficiencies.

ALESEA plays a key role in sustainable logistics by minimizing reel loss, extending the lifecycle of materials, and reducing the need for new production. This leads to less waste, lower CO₂ emissions, and a smarter, greener supply chain.

About E Path

We provide products that are the green life blood that brings energy and communications to homes, infrastructures and cities around the world.

With a business strategy consistent with the UN Sustainable Development Goals, we strive to be green inside. We express this through products that when installed in homes, infrastructures and cities around the world, make these just as green inside.

E Path goes beyond cables, embracing services and projects consistent with our strategy to be a solution provider.