The offshore production of oil and gas plays a vital role in the energy infrastructure of many countries.
However, operations around this production can be extremely energy-intensive. On larger and more complex platforms, for example, the on-site energy requirement can be up to several hundred megawatts.
Prysmian has more than proven itself in this sector.
In addition to a comprehensive package of AC and DC cables, we supply products for the transmission of onshore electricity to offshore platforms via submarine cable systems.
Our efficient connections supply offshore oil and gas drilling rigs with constant and reliable power. At the same time, they offer an environmentally advantageous solution by eliminating local energy generation, typically based on diesel, on the platforms. Electricity from the national grid is also cheaper than electricity generated by diesel, so that this solution is also economically attractive.
With our end-to-end service and innovative backup of production, installation and engineering assets, we are a single-source provider and can meet our customers' needs with total solutions for EPCI turnkey cable systems.
Our entire value chain sets us apart, providing our customers with a single point of contact with no hassle for all their project needs.